This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS613221AEVM: True shutdown for TPS613221ADBV

Part Number: TPS613221AEVM

I'm using a load switch for true shutdown of the TPS613221ADBV boost converter (it doesn't have an enable pin). I am currently using the Renesas SLG59M1551V load switch, which has 15.5 mOhm internal resistance. My current draw on the boost converter averages around 10 mA. Would you be able to tell me if that load switch is acceptable for this purpose? I'm not able to accurately measure the efficiency of the boost converter, but I followed the design suggested by WeBench and it seems that the efficiency I'm getting may be somewhat less than the 85% that WeBench calculates. Thanks very much!