Hello experts.
The data sheet says "The charge OCP threshold is automatically set to 6, 9, and 12 A on a 10-mΩ current sensing resistor based on charge current register value."
Could you tell me the threshold to be set to 6, 9, and 12 A?
【charge current】 【OCP】
2.8A → 6A? 9A? 12A?
1.3A → 6A? 9A? 12A?
0.8A → 6A? 9A? 12A?
0.5A → 6A? 9A? 12A?
0.3A → 6A? 9A? 12A?
Thanks and best regards.
Tomoya Yoshino