I have designed a boost DC-DC convertor circuit using LM3478. The input voltage is 12V,13A (via AC-DC Power Supply) and the output voltage 24V,5A. Circuit has been worked fine for few days and suddenly the convertor is not working and it is supplying the same input voltage at the output side (11.76V). I have checked the frequency and i am able to read 110kHz. I have also replaced the LM3478 and the Inductor but it is not working. Can you please guide us what could be the major issue in this,
Please find the schematic for your reference,