Other Parts Discussed in Thread: LM5169
Hello,
We are designing a multi output power supply using the LM5168F with the following specs :Input : 20 – 60Vdc. Out1: 5V/50mA non-isolated, Out2: 6V/150mA, Out3: 6V/50mA
Using the datasheet and spreadsheet calculators - L = 66uH for selected Fsw = 680KHz. Hence we designed the transformer with higher L of 80uH.
The output are generated but the voltage for Out2 drops for 20Vin and full load. Full load is supported beyond ~45Vin.
Next we changed the transformers to two new types(2 & 3) as below and tested again.
1. L = 80uH, AL = 90 (first version we tested)
2. L = 124uH, AL = 145, same turns as 1,primary turns split 50-50, higher L achieved by using higher AL core
3. L = 90uH, AL = 90, higher turns than 1 & 2, primary turns split 50-50, same core as 1, higher L achieved through higher number of turns
Support for full load is best with 124uH transformer except slight drop for Out2 at 20-24Vdc. Drops are much lower for 90uH transformer also compared to type 1.
Does this indicate that L values below 125uH are not able to transfer adequate energy to the isolated secondaries?
If yes, please suggest the L we should try next - around 150uH?
Also, to achieve this there are two options - more turns or higher AL - which is preferable?
2nd query: Please advise the recommended voltage rating for Ca and Cb for a max Vin of 60V.
Best regards,
Tanmay.