Hi I want to drive LM3644 using MCU. My strobe signal from Camera is connected to LM3644.
TX Pin diasbled 0
Strobe type 0
Strobe enable 1
Torch pin 0
Mode IR drive 01
LED2 off 0
LED 1 ENABLE
0x25 my enable register value. There is no connection error between IC and MCU, There is no error flag from the flag registers.
Where could I doing mistake at ? My IR laser is not working.