This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Best buck controller IC's for constant current power supply

Other Parts Discussed in Thread: LM5145, LM5149, LM5148

Good morning, i need to design a constant current power supply with the following specs:

V input: 60V 

Vout: 0-48V

Iout:0-10A

 I need it to be adjustable and i was thinking about using an LM5145 and change the feedback loop to make it work in constant current mode. After many simulations with PSPICE i dont have a good result, so im wondering if there are more suitable IC's for this purpose.

Thank you.