I want to use a LM3553 to drive a string (series) of 2 white LED in a camera flash application. Input voltage is 5V.
I understand that maximum ID1+ID2 = 1.2A which corresponds to Rset = 14kR.
By setting bit ST1=0 and bit ST0=0 the stepping time is 25us so for the LED current to increase from 0 (I don't use torch mode) to 1.2A the ramp would take 128 * 25us = 3.2ms.
What if I needed a faster ramp? Could I use Rset = 7kR and only set FC6-FC0 < 64?
Would the LM3553 be able to ramp up the output current to 1.2A in 64 steps corresponding to 1.6ms?
How fast can the LM3553 actually ramp-up to 1.2A?