This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: GPCCHEMID Report

Part Number: BQ34Z100-R2
Other Parts Discussed in Thread: BQSTUDIO, BQ27426

I tried GPC Chem ID tool by logging the data using BQstudio. My cell is Li-ion (LFP) with 280Ah capacity

I am pasting the results of GPC report, do you see any concerns? Or should I just use the Chem ID 481 as suggested by the tool

Chemistry ID selection tool, rev=2.54

Configuration used in present fit:
ProcessingType = 2
NumCellSeries = 1
ElapsedTimeColumn=0
VoltageColumn = 1
CurrentColumn = 2
TemperatureColumn = 3

Best chemical ID : 481 Best chemical ID max. deviation, % : 26.23



Summary of all IDs with max. DOD deviation below 3%

Chem ID max DOD error, % Max R deviation, ratio
0 0 0

Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule


Selection of best generic ID for ROM based devices like bq274xx


Device / Family #1
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
354 bq27411-G1C: 4.35V LiCoO2 32.13
3142 bq27421-G1D: 4.4V LiCoO2 38.92
128 bq27421-G1A: 4.2V LiCoO2 50.67
312 bq27421-G1B: 4.3V LiCoO2 99.07
Best generic ID 354
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule


Device / Family #2
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 32.13
1202 bq27621: (default) 4.2V LiCoO2 32.21
1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 35.72
Best generic ID 354
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule


Device / Family #3
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
3230 bq27426: (default) 4.35V LiCoO2 31.09
1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 32.21
3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 38.92
Best generic ID 3230
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule