TPS84320の出力についてご教授いただけると助かります。
FPGAの電源用としてTPS84320を使用しているのですが、出力波形にパルス状のノイズ?が見えている状態です。
波形と回路図を添付しますので、何かアドバイスがいただけると助かります。
尚U402はシンボル上は1.03Vとなっていますが実際は0.95Vです。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS84320の出力についてご教授いただけると助かります。
FPGAの電源用としてTPS84320を使用しているのですが、出力波形にパルス状のノイズ?が見えている状態です。
波形と回路図を添付しますので、何かアドバイスがいただけると助かります。
尚U402はシンボル上は1.03Vとなっていますが実際は0.95Vです。
Thank you for your comment.
Below is a machine-translated version of the full text.
--from here
It would be helpful if you could teach me about the output of the TPS84320.
I'm using the TPS84320 for the power supply of the FPGA, but I can see something like pulse-shaped noise in the output waveform.
I will attach the waveform and circuit diagram, so it would be helpful if you could give me some advice.
U402 is 1.03V on the symbol, but it is actually 0.95V.
--to this point
Sorry for the inconvenience, but thank you in advance.
Hi
The noise looks like measurement coupling. Would you mind use pig tail to test, and let the probe connect to the output cap directly.
Shuai