Other Parts Discussed in Thread: LM4853,
Hello, I am using a TPS61202 to supply 5V to an audio circuit (utilizing the LM4853). I'm following the reference schematic in the TPS61202 datasheet: 2.2uH inductor with 2A saturation current, 22uF input and output capacitors, 25V, X5R. Input voltage is anywhere between 2V and 4V, the issue remains no matter the input voltage (tried both bench power supply and lipo battery). I'm measuring voltage right at the output of the converter.
What I see on the scope, when the volume is turned up (not too high, only 100s of mW at most), I can see the audio waveform imposed on the 5V rail. If loud enough, the ripple voltage can reach past 100mV peak to peak. The TPS61202 datasheet indicates a Load Regulation of 0.5% max, which would be 25mV, correct?
Is this not the correct specification I should be looking at? I didn't expect low frequency ripple voltage to be an issue on the converter. What can be done to decrease this ripple?