This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51420: Ringing during transient load change

Part Number: LMR51420

Hi,

I'm currently designing a boost converter around the LMR51420. Output current = 0.9A, L = 10uH, COUT = 2x22uF, R1 = 100k, R2 = 13.7k.

It seems that when the load is changed from 0 to 0.9A, there is a large spike (5.3V, usually voltage is at 5V). Is there a way to minimise this by adding a feedforward capacitor? There doesn't seem to be any guidance in the datasheet. Would you be able to suggest how I can remedy this?

Thanks!