These three descriptions in the manual are not very clear, please help to interpret them, thank you
1. When working in PWM mode, why should minimum open time and minimum close time be considered when setting frequency through COMP/FSET's resistance to the ground?Is the specification of ton and min referred to the upper tube or the lower tube?
2. As shown in the screenshot below, what does V represent in the formula for calculating the minimum output capacitance?Does it mean the input voltage?
3. What is the internal structure of COMP/FSET pin?In R11002 and a 10 nF capacitor, the PWM frequency at SW end is relatively stable, R11002 and a 100 nF capacitor, the PWM frequency at SW end is in variable frequency mode