This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2HB50-Q1: ICL(min/max)

Part Number: TPS2HB50-Q1
Other Parts Discussed in Thread: TPS2HB35-Q1

Hello,

The datasheet specifies ICL(typ)=11.8A at RILIM = GND, open, or out of range.
My customer would like to know ICL(min) and OCL(max) at the same conditions.

Best regards,

K.Hirano

  • Hirano-san,

    When the ILIM pin is open, we consider this a fault condition where the resistor that should be on the ILIM pin has lost its connection. As such, we do not have data for the minimum or maximum current limit. At this point, all we guarantee is that the device will shutoff and protect itself in the event of a current limit or short-to-ground situation. 

    If you need a higher bound for min/max current limit, the recommendation is to use the B version of the device or swap up pin-to-pin with the TPS2HB35-Q1.