This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31710: PCB layout and stress question

Part Number: LMZ31710


Hi Team,

On customer PCB, LM31710 is very close to a screw hole. The diameter of screw hole is 3.5mm. The distance from the edge of module to the center of screw hole is 5.5mm. Customer concerned about the stress issue. So I was wondering if there is any restriction about the distance between module and screws. Could you pls give some comments on it? Thanks!

Rayna