This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606EVM-897: Chip and EVM Components Damaged During Hot-Plug Despite Following Datasheet's Advice To Add a Schottky Diode

Part Number: BQ79606EVM-897


I have fried the BQ79606AQ1 Chip as well certain EVM components around cell 1 and certain power supply filter capacitors. I believe the issue has to do with the problem described in section 9.2.1.2.6 CB Input of the chip's datasheet, which states:

The Cell Balancing input are connected to internal balance FET through balancing resistor. The resistor sets the balance current. Connect CBn to VCn if not used. The CB pins must NEVER be connected to cell voltages (module connectors) that are expected to be less than the recommended operating condition. The internal FET diode will conduct and likely damage the FET in reverse voltage conditions. CB0 can not be left floating at any condition. If a connection to cell1 negative terminal is open the IC bias current will flow through the CB1/VC1 pins and then to the cell2 negative module terminal, causing CB1 and VC1 pins to go below the minimum voltage recommended with respect to pin AVSS. This violates device spec. If the module connector ground pin can float while the other module terminals are still connected it is recommended that a schottky diode be added between CB1 and device GND (AVSS) to ensure that CB1 and VC1 pin voltage does not violate the absolute maximum limits.

Despite the fact that I have added the schottky diode as specified and have confirmed that this prevents the issue from occurring in the past, I believe the issue has occurred again and I would like an explanation of how this is possible given the conditions of the failure:

  • The battery has 6 cells and jumpers J2 and J3 were connected to use the battery as the chip's power supply. The resistor ladder switches of SW2 were all OFF.
  • The wires for cells 1-5 were wired to the EVM J1 connector and the cell 6 terminal was left floating. Note that the battery side connections were not made as of yet.
  • Cells 1-5 were then all instantly connected to the EVM by connecting the battery side input connector.
  • After about 30 seconds, there was smoke and the cells were disconnected from the battery side. Note that the chip was not expected to be operating after the connection was made as the MCU that controls its operation through J8 was powered off the entire time.
  • Resistors R34, R35 and R28 were damaged, with R34 being cut in half and R28 shooting up to over 20k ohm. 
  • Capacitors C4, C5, C9-11, C40, and C55 were all damaged as well and require replacement.
  • The conductor from the J1 cell 0 terminal to J3's short to EVM ground was stripped of insulation and severed.

I strongly suspect that the problem described in section 9.2.1.2.6 is the issue because of the damage to resistors and capacitors around the lowest voltage cell that is not replicated anywhere else other than at the power supply filter capacitors. The damage includes external components from both the CB1 and VC1 circuits. Is there an explanation for why keeping cell 6 floating and instantly connecting cells 1-5 would cause this, despite the schottky diode being in place?

  • Good morning,

    Thank you for reaching out to us. Some of the things to point out is to make sure that the unused CB and VC pins are shorted properly. Also, a hot plug of the batteries could cause a voltage and current spike on the device.
    You stated that you have confirmed that adding the schottky diode has prevented the issue in the past. Another probable problem could be that the BQ79606 device could have had ESD damage or a burnt component before you connected the battery cells.

    Best,

    Fernando Dominguez

  • Hi,

    Is it a requirement that cell 6, acting as the BQ79606AQ1 power supply, is not floating during a hot plug of the other cells? I have not experienced any issues when hot plugging all 6 cells in the past. 

    What procedure is recommended to wire the 6 cell voltages to the EVM? I have previously wired this exact battery with no issues by connecting the battery side connector first and then wiring the 6 cell voltages to the EVM one-by-one from the lowest voltage to the highest voltage.

  • Hi Steven,

    If you have a schottky diode this one usually protects cell 1 (VC1/CB1) from negative transient voltages since sometimes during a hot-plug event like the one you are causing the voltage on these pins can fly negative for a short period in time.

    I think your issue might be a bit different, since you are not connecting the top of Cell 6 (power supply to the device) the current flows from cell through the back-body diode of the cell 6 FET and it is trying to power the device through it. This is why we usually recommend that GND and top most voltage (in your case CELL6) are connected first and then all cells in between.

    Regards,

    VIktor.

  • Hi,

    Could you please direct me to documentation where the recommendation for connecting the battery to the evaluation module is? The IC is advertised as being designed for hotplugging, but according to the datasheet not all of the parts required for safe hotplugging are present. 

  • We don't have a documentation for this as each customer system is different and different protection components are used.