Part Number: BQ2980
Other Parts Discussed in Thread: BQ25175,
Hi Team,
customer is looking for a protection IC with following specs.
Could you please recommend a suitable solution?
- Overcharge detection voltage: >4.393 (max value of BQ25175)
- Over discharge detection voltage_ between 2.7V >= and <3V
- Adjustable max current of up to 3A (min)
- Should be able to detect shorts and disconnect battery.
- need a dedicated input pin for connection with MCU. Goal is to disconnect the battery and when charger is connected (USBC 5V, via BQ25175 4.35V) the battery automatically gets connected again.
Battery is a 1 cell LiPo, HV 3.85V 30mAh
BR,
Stefan