Hi
We are encountering a weird behaviour on the PTR08100W power module and would like to seek for advise.
We have built the circuitry for 5V output with this power module using the following:
Cin --> 1 x 330uF(recommended electrolytic capacitor EEUFC1E331)
Cout --> 1 x 330uF(recommended electrolytic capacitor EEUFC1E331)
Rset --> 255ohm (2 x 510ohm resistor in parallel)
This 5V (5.22V) will be used as an input to three other linear regulators that each have an output current of up to 3A.
Our board works successfully with the Vin of the PTR08100W at ~5.0-5.3V (external power supply that can output up to 3A).
However, when the Vin of PTR08100W is increased above 5.8V, we observed that the current drawn from the external power supply will drop in the middle of our operation and our operation will fail. The current did not change when the Vin was at ~5.0-5.3V.
Attached is a .doc with the table of the experiment that we did.1070.PTR08100W_current_issue.doc