Hello,
we want to implement direction dependant current limiting. For example a battery with max. 1.5 A charging and 4 A discharging. Additionally a signal should allow to disable one direction, whilst still allowing the other.
Is this possible by using two TPS25947 in anti-parallel configuration?
My understanding is that the IC can limit up to 5.5 A, but the 62368-1 certification is only applicable up to 3.96 A continuous. What does "Output Current Limit: 0.575 to 4.84A" mean?
Sincerely
JK