Other Parts Discussed in Thread: TPS22967, TPS22953
Hello Team,
I am using the TPS22975N as an inrush current limiter. It is used to charge a big capacitor (2,000 µF) used as an energy tank for our system.
This design have been made following all chip recommendations but CIN/CL which should be greater than 10. As a matter of fact, CT is set to 10 nF which limits the current to less than 900 mA at any moment: this current can easily be provided by our primary power supply block.
Do you confirm our assumption is correct ?
Do you detect any flaw in our schematic ?
To finish with, at power-up there is a transient state during which (Vin-Vout).Iout rises up to 2 W for 10 ms or so. I haven't found the usual power transient derating curves in the datasheet: can the component handle such a peak for this little time ?
Thanks in advance for your reply, regards,
Mathieu