Other Parts Discussed in Thread: BQSTUDIO,
I have been reading and I haven't found a way to use the PDSG FET autonomously.
By default DSG is on in SLEEP which means current is available to drive a load. When that load exceeds either Power:Sleep:Sleep Current or Power:Sleep:Wake Comparator Current then the state transitions to NORMAL.
What I would like to do is have PDSG FET enabled instead of DSG FET and, when the load is first applied and a small value in Power:Sleep:Sleep Current or Power:Sleep:Wake Comparator Current moves the state to NORMAL then the pre-discharge timer and/or predischarge stop delta voltage sensing commences (according to their settings being non-zero).
That way, on first connection of the load, the PDSG FET is ready to limit inrush. In the present settings, with DSG FET enabled, the inrush cannot be avoided because it may be up to 48mS before the load current is sensed and it is most likely the inrush has already happened.
I can't see any way to use PDSG FET other than by register updates from a host MCU. Is this the case or am I missing the correct register settings ?
Al the best
Harry