This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: Design review

Part Number: LM5175
Other Parts Discussed in Thread: LM5176, TPSM5601R5H

Dear Support, my design (name: 56000080200) has this specification : Vin=20-30V, Vout=24V, Iout=20A, max ambient temperature 60°C (based on LM5175 or LM5176). Typical operating condition (24/7/365, every day) is Vin=24V, Vout=24V, Iout=8A but, in same conditions Vin can go down / up until 20V / 30V and Iout can become 20A; so I design it for Iout=20A and my target is to reduce LM517x power loss. I need design (schematic) review so I want share schematic, part list and my questions. Can you send a mail (or other) to attach documents ?