Other Parts Discussed in Thread: TPS7A26,
Is it recommended to use TPS7A26 +3.3V output as VCC for LM3880 and the Power-Good output of the same TPS7A26 as the "External Enable signal" as illustrated in Figure 8-5 on Page 16 of LM3880 datasheet?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In my application with a single +12V DC input supply, I am not able to design the power-down sequencing with LM3880. When the +12V supply is turned off the VCC to LM3880 will also be off, so the power down sequencing which is controlled by the enable signal will not work. Please suggest.
Hi Soumyadeep,
I don't quite understand. Are you asking for a solution where the VIN is off, but still has a VCC to power the LM3880?
Best,
Ryan
Hi Ryan
Thanks for your reply. Yes, if the single VIN (+12V) is suddenly turned off, is there any way I can do the power-down sequencing with LM3880 without any other separate VIN to power the LM3880? Actually I was planning to use the TPS7A26 to generate the +3.3V and PG signal from +12V VIN. This is ok for the power-up sequence as you confirmed in your earlier reply. But then I realized that power-down sequencing may not work with this scheme because the +3.3V VCC of LM3880 will also instantly turn off along with +12V. My application is to sequence the drain and gate voltages of RF power amplifiers during power on and power off. Any suggestions will be great.
Thanks
Hi Soumyadeep,
I do not think you can. When you power down the VIN there will be no other source that can power the 3.3 V for VCC and PG for enable.
Best,
Ryan