This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61181AEVM-259: TPS61181A

Part Number: TPS61181AEVM-259
Other Parts Discussed in Thread: TPS61181EVM-259, TPS61181A

Hi,

We are doing tests on a TPS61181EVM-259 board from which we have removed the jumpers, so that the IFB pins are not connected to Gnd.

The supply voltage is 13.30V and we used series of 6 white leds (18.90V when on).

In first test we used one series of leds on IFB1, and one series of leds on IFB2 with IFB3 to IFB6 unconnected.

We tested concretely what is referred to in the manual in

After set Enable pin, Vo reaches the maximum voltage and the leds turn on, the voltage starts to decrease until it gets close to 0V, and the leds turn off definitively.

The leds stay on only for a few seconds.


We tested several configurations with jumpers, but it is enough that at least one IFB pin is disconnected from Gnd for what was described to happen.

As we cannot use jumpers on our board, and we have a problem that we don't know how to solve in order to use a variable number of IFB pins with leds.

Any comments would be appreciated.

regards

Jose