Hello team,
I want to use TLVM13630 for 5Vin -> 4Vout (which is 80% Duty).
From the datasheet Table 7-4, the Vout range when VIN=5V is limited only to 3.5V.
I have calculated the MAX DUTY from the Minimum OFF time and Max ON time of the FET, which was >99%.
Why is the Vout range limited to 3.5V, when VIN=5V?
Best Regards,
Kei Kuwahara