Hi,
Good Day.
I am trying to build a power converter, using GaN Hemts.
Therefore, I chose your isolated gate driver UCC5304 as it is one of the few isolated gate drivers dedicated to high-voltage GaN technology out there (I am using 1200V GaNs).
Now, the data sheet says that the supplied isolated voltage (VCC) can be anywhere from -0.5 to 20V but the recommended operating area is 6...18V.
My GaN Hemts do not accept a voltage greater than 7.5V. Thus, my VCC probably should be between 6 and 7.5V, even though that is already a pretty narrow span, considering that 7.5V is the absolute maximum rating of my transistor.
My question is, why the datasheet recommends a voltage of 6...18V, and what bad could happen if I operate the driver with only 5V. Because I want to use an integrated circuit as the power supply for VCC and most manufacturers offer ICs that generate 5V and not 6V.
Since most GaNs need a lower gate-source voltage than MOSFETs, I am actually surprised that the recommended operating region for VCC is 6...18V for this GaN-Hemt driver.
Please advise. Thank you very much.
Best Regards,
Ray Vincent