Hello,
During our test, I found power efficiency is very low and only up to 20%. Vin=13.5V, Vout=3.3V, Iload_nor=20mA, Iload_max=60mA.
Baesd on datasheet, efficiency should be up to 65%. I also did a simulation with inductor using Murata dc-dc convert tools. The results
showed efficiency is about 89%. More strangely, based on my test data, the SW frequency is 1.022MHz but TPS560540YQDBVRQ1 frequency should is 2.1MHz based on datasheet.
Pls find my SCH design and test data, help to check what happened and how to improve it.