This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS564247: Thermal Issue

Part Number: TPS564247

I am using TPS564247DRLR for 2.8VDC with a maximum load of 2.5A in worst case peaks.

Nominal current is usually 100mA at the 2.8V output. Still i have done all the tests with 2.5A to have a worst case temperature rise.

 

I have considered rja=70deg to get this rise.

In practical i could confirm the same.

Now my point is whether this IC not rated for this high current at 2.8V output, or can i still reduce the temperature with Layout modificationsince i need to operate it upto 70deg ?