Part Number: CSD25501F3
Other Parts Discussed in Thread: CSD25485F5
Dear Team,
Do you have pin to pin replacement of 703799-00 SHANGHAI BELLING,BLM3415?
|
SHANGHAI BELLING |
BLM3415 |
XSTR,MOS,SOT23,-20V,-4A,PCH,60/47mOHM |
Thanks a lot.
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CSD25501F3
Other Parts Discussed in Thread: CSD25485F5
Dear Team,
Do you have pin to pin replacement of 703799-00 SHANGHAI BELLING,BLM3415?
|
SHANGHAI BELLING |
BLM3415 |
XSTR,MOS,SOT23,-20V,-4A,PCH,60/47mOHM |
Thanks a lot.
Jimmy
Jimmy,
The SOT-23 package is not something that TI offers for MOSFETs.
The closest device we have to this BLM3415 device would be the CSD25485F5.
The TI device is a Silicon package 1.2mm2 vs 7,5mm2 plastic package from competition, so we are much smaller.
Our max resistance is 42mOhm @ 4.5Vgs vs comp 47mOhm, so we are a little lower resistance.
Our leakage specifications are much better, if this is important to the customer, we are 20x lower Idss and 400x lower Igss.
Thanks
Chris....