This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD18509Q5B difference between NexFET and GANFET

Hi,

what is the difference between NexFET and GANFET?. Shall we use GANFET instead of NexFET for drone application?

  • Hello Yogini,

    Thanks for the inquiry. TI NexFETs are silicon power MOSFETs. A GANFET is a gallium nitride (GaN) FET. At this time, TI does not make any discrete GaN devices. Unlike our discrete power MOSFETs (NexFET), all of TI's GaN products integrate the driver and the 600V to 650V GaN FET into one package. Discrete GaN FETs are available from other semiconductor companies but are typically higher cost than silicon FETs. GaN devices are typically lower charge than comparable silicon FETs and can be operated at higher switching frequencies. Silicon FETs are still very cost competitive and offer good performance in motor drive applications.

    Best Regards,

    John Wallace

    TI FET Applications