This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4510: LM4510SDX/NOPB

Part Number: LM4510


Is it suitable to use LM4510SDX/NOPB for the following application.

Input Voltage Range:3-4V

Output Voltage: 12V

Output Current: 200mA or more

  • Hi Parvathy,

    Sorry for reply late.

    LM4510 is suitable for the application.

    please be careful at 3Vin 12Voout 200mA it almost reaches the minimum current limit 1A.

    It is recommended to leave some margin.

    Best Regards

    Fergus