Other Parts Discussed in Thread: BQ40Z50, , BQ30Z55, BQ4050, EV2400
Hello E2E Experts,
Good day.
- Could you help me unseal the chip BQ40Z50 installed in the HP battery SS03XL?
Device type 4550_1_05, I think it is BQ40Z50-R1
The default unseal keys 0x0414 and 0x3672 not working for it.
Additional information:
I have the ASUS laptop old batteries with the chips BQ30Z55 and BQ4050. I haven’t the problems to unseal it and change parameters, they have the default unseal keys.
I also have the HP problem battery SS03XL with the chip BQ40Z50-R1 (4550_1_05) and I can’t unseal it with default unseal keys 0x0414 0x3672. As I understand the chips BQ4050 and BQ40Z50-Rx have the same unseal/FAS procedure.
I have the device CP2112 and my own C++ program. And I have the device EV2400 and the application BQ Studio.
Any help would be appreciated.
Regards,
CSC