Hi
My customer is designing LMG3410R150RWHR.
It is said that the pins below are not used.
-unusde pins-
pin 25(LDO5V) , pin 26(VNEG), pin28(BBSW), pin29(LPM), pin30(RDRV), pin32(FAULT)
I want to know how to handle it.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer is designing LMG3410R150RWHR.
It is said that the pins below are not used.
-unusde pins-
pin 25(LDO5V) , pin 26(VNEG), pin28(BBSW), pin29(LPM), pin30(RDRV), pin32(FAULT)
I want to know how to handle it.
Thanks
Hi,
If the customer is not using the following pins, here is how they should be connected -
pin 25(LDO5V) - Connect a 1-µF bypass capacitor from this pin to source
pin 29(LPM) - should be tied to pin 25(LDO5V)
pin 32(FAULT) - it is an output pin, so can be left as is i.e., floating/open
The following pins need to be configured according to the datasheet.
pin30(RDRV) - Connect a resistor from this pin to source to set the turn-on drive strength. The value of the resistor determines the slew rate of the device during turn-on between 30V/ns and 100V/ns. Figure 2 from the datasheet provides the RDRV vs slew rate information.
pin 26(VNEG) - Connect a 1-µF bypass capacitor from this pin to source
pin28(BBSW) - Connect an inductor from this pin to source. A TDK Corporation VLS201610HBX-100M-1 10 µH SMT inductor in a 0806 package is recommended. This inductor is required to complete the internal buck boost converter which generates a negative voltage necessary to turn off the device.
Thanks,
Nanditha