Other Parts Discussed in Thread: UCC28911, UCC28910, TLV767, TLV761
Hi team,
Does UCC28881 support 7V output with 200mA~300mA load in non-iso flybuck topology? As read from datasheet, the limitation is 225mA in open frame design. Where is the output current limitation coming from? Also is there any limitation on output voltage? (I imagine higher output voltage can reduce output current.)
In addition, Is above same in UCC28911?
Regards,
Hayashi