Hello Together,
We are using this part TPS7B8150QDGNRQ1 in our C-Sample phase with the below configuration.
UBD_VP_PI is the reverse voltage and transient protected automotive battery voltage.VDZ5_PERM is 5V which is present always even during the sleep mode.
Output (VDZ%_PERM) has very lighter load and hence to protect the OUT PIN during OFF scenario (If Input voltage discharges faster than output voltage), we have used a protection diode D3280.
1. Please let us know if we have body diode present inside the chip itself or not?
2, Do we really need diode for this part?
Regards,
Arun.
Bosch.