Other Parts Discussed in Thread: TPS65235, TPS65235-1
Hi,
I use TPS563211 to convert input 5~10V to 3.3V, exact the same circuit as reference design in datasheet.
The circuit works but, when the board is laid on top of a flat surface, like a table, it will generate audible sound, and it looks come out from the inductor. However, when the board is like handheld or mounted on a rack, no sound can be heard.
What could be the possible reason?
Thank you.
/Roland