Hello team,
The output ripple measurement graph (Fig 1) is very different from the output ripple calculation equation (equation 4) on the datasheet.
The shape of the graph on Figure 1 is not linear. What is the condition of the circuit used in this measurement?
There seem to be several drop points Do you change the Cout value during this whole measurement (Iout: 0.0001 to 1A)?
I have substituded the below parameters to the equation 4 of the datasheet.
COUT = 2.4 uF @5V, ESRCOUT= 3.5 mΩ, fSW = 2 MHz
The Vripple vs IOUT graph drawn is below.
This graph is very different from the shape of the Figure 1 shown below.
Best Regards,
Kei Kuwahara