Other Parts Discussed in Thread: LM3410
Hello,
I'm considering an LED driver with the following specs.
I think the TPS61193 will meet the requirements, but this product does not have a SEPIC evaluation board.
Do you have a product that meets the following specifications and has an evaluation board that allows you to consider the conditions?
(Specification)
VIN: 18V to 29V
VOUT (VLED): 16.4V to 25.6V
ILED: 80mA (only 1ch)
Dimming Ratio: 6000:1
Best regards,