This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27411-G1: Pulsed discharge current

Part Number: BQ27411-G1

Hi,

we are planning to use BQ27411 (or similar) as a  fuel gauge.

The discharge current will be PWM with 2kHz and Imax 1,5A.

The data sheet says ADC conversion time is 1s.

Will the pulsed discharge current lead to big inaccuracy?

Thanks and regards,

Carsten