Hi,
I'm using TPS25200QDRVTQ1 in my design and I need to use the ENABLE pin. It seems from datasheet that the turn ON threshold is 1.9V and also I noticed about the 330mV hysteresis but the system that gives me the EN logic voltage is only 1.8V. Would that work fine? Or does it mean I need to use a level translator?
I did check working of the ENABLE pin on a different design that uses it and provided a 1.8V and it worked fine all the way up to 1.48V but is it reliable since there's a mention of 1.9V in the datasheet? I'm in a situation where I don't have any other voltages other than the input voltage coming from host power supply and this 1.8V logic ENABLE.
Please advise