This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568215: PGOOD Output

Part Number: TPS568215

Hello,

I'm referring to the following two E2E threads regarding TPS568215's PGOOD output performance, off-leakage current and internal on-resistance, but can I consider the values in those two threads those under full temperature range?

  • TPS568215: PGOOD spec
    • This thread says, "..., add 100% margin, max is <200 ohm."
  • TPS568215: PGOOD Leakage Current
    • This thread says, "..., suggest you can take 500nA to reserve some buffer."

Best regards,
Shinichi Yokota