Other Parts Discussed in Thread: TPS2121
Dear Sir/Madam,
We found that TPS2120 does not seem to be working correctly. From below graph, Both source 1 &2 are connected to USB-C 5V, when source 2 is unplug, the output dip and cause the system to reset instead of seamless swapping over of power. But the output remains constant when source 1 is unplug.
And, if plug in source 1 first, then plug in source 2, the output will drop like below. Can you advise?
The output is OK when either source 1 or source 2 is plug in.
Best Regards,
felix