Other Parts Discussed in Thread: LM5149, LM5148
I'm a engineer from ABB robot R&D
The application is 48V ->24V
the problem is when I apply 0.1A load to 24V, the output can't rise, can only rise to 0.3V.
but however when there is no load to 24V, the output can rise to 24V.
I check the EN, it is ok, the under voltage threshold is 34V.
the chip is not hot at all.
when I check over current, I set over current threshold is 6A, the shunt resistor is 10 mΩ. although I check the real current, it is only 0.5A now over the inductance L35.
the schematic is below:
the failed power on process, you can see the output can't rise. (with 0.1A load)
C1: current of inductance L35
C2: D-S voltage of lower MOSFET
C3: VIN
C4: VOUT

the successful power on process, you can see the output can't rise. (with no load)
C1: EN pin voltage
C2: D-S voltage of lower MOSFET
C3: VIN
C4: VOUT

the MOSFET on time is quite short like 0.4us and have long off time at the failed power on case.
see below.
C1: current of inductance L35
C2: D-S voltage of lower MOSFET
C3: VIN
C4: VOUT

looking forwards to your answers. thanks!