Other Parts Discussed in Thread: TLV755P
Hi experts,
I believe that VIN < VEN may occur in the application of my customer's product under development. Could you please answer the following questions about the TPS7A03 behavior when VIN<VEN?
- Is it correct to understand that "In the situation of VIN<VEN (eg VIN=0V, VEN=3.0V), the consumption current increases, but it does not affect the reliability or damage of the product".
The customer thinks as above from the fact that the absolute maximum ratings of Vin and Ven are stipulated independently, and from the behavior of other LDOs such as TLV755P. TLV755P datasheet 7.3.2 clearly states that VEN current increases when VIN<VEN suggesting that there is no problem in use if the user can tolerate an increase in the current of VEN. Is it the same for TPS7A03?
Thank you for your help.
Regards,
Taito Takemura