This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62130: TLV62130 Pin2Pin Alternative Recommendation

Part Number: TLV62130
Other Parts Discussed in Thread: TPS62110

Hi TIer

Do we have a chip which pin2pin TLV62130 and its output voltage include 7V?

Customer want to find a chip like this. I do not find it on Ti .COM.

I think the current advanced technology has improved heat dissipation, and they all use new pads.

Is my understanding correct?

Could our TLV62130 can output 7V , D/S is 5.5V?

Thank you very much. Looking forward to your reply.

  • Hi Yuxi,

    We don't have P2P device of TLV62130 which can support 7V output.

    TPS62110 is a 1.5A part with the same package and can support 7Vout.

    Could our customer accept other devices not P2P? If so, I'll recommend some suitable ones.