Hi,
As per TPS61240-Q1: Output Current Limit - Power management forum - Power management - TI E2E support forums, the output current supported is upto 240 mA, but simulation shows that the device is unstable (considerable noise) when tried to drive at 230 mA resistive load. With no load connected, the output looks perfectly OK.
Please guide on what went wrong.
Simulation circuit

The input and output capacitors used 10 uF each while the inductor used is 10 uH.
Simulation result

Kindly help to understand this behavior.
Dixit