Part Number: BQ25896
Other Parts Discussed in Thread: BQSTUDIO
Hello,
I want to use the BQ25896 in a hot ambient environment (40°C). Our battery has a max charge temperature of 45°C and contains a 10KΩ Thermistor with a Beta of 3435. Whenever the battery temperature reaches the JEITA T3 level of 45°C the VREG voltage is set to a value of 4.0V (VREG(4.2) - 200mv = 4.0v). This is expected as we have the JEITA_VSET bit set to 0. What is unexpected is this appears to put the IC into the constant voltage phase of the charge cycle. The battery continues to charge until it reaches our charge termination value of 256mA when the BQ25896 terminates the charge cycle and indicates a completed charge. The battery however is not charged to 100% and confuses the user into thinking it is.
Am I correct that the BQ25896 is in constant voltage mode when it hits the JEITA T3 value with the JEITA_VSET bit set to 0?
I know I could gain a little more capacity by setting the termination current to a lower value or allow charging at higher temperatures, by setting the JEITA_VSET value to 1, but are there any other register settings (see attached from bqStudio) that I could change to allow for a complete charge of the battery at 40°C ambient?
Is there something I'm not considering that could help me?
Thanks,
Rob