Other Parts Discussed in Thread: GPCCHEM
hello , can you explain me why The chemical selection doesn't match from our cells to your power calculator GPC ?
here is the file we use for it, it is a M35A cell from Molicell
regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello , can you explain me why The chemical selection doesn't match from our cells to your power calculator GPC ?
here is the file we use for it, it is a M35A cell from Molicell
regards
Hey Gus73220,
I looked over the files you sent and I do see one issue with how the test was performed. The charging and discharging was done at a higher than recommended rate. You charged at 5A and discharged at 1A. It is recommended to charge at a rate of C/2 and discharge at a rate of C/10. Therefore, I would recommend you to redo the test, but this time, charge at 1750 mA and discharge at 350 mA (since the capacity of your battery is 3500 mA).
Sincerely,
Nick Richards
Hey Gus73220,
Sorry, I should have clarified with you, are you running multiple cells in parallel?
The GPCCHEM is going to try to match it best with all the cells that we have characterized. Therefore, there are many aspects that can affect the results of the test, including temperature. If the temperature that your test was run at is more or less than room temperature, then this can be the cause of your battery being matched to a different cell. I did notice that the temperature of your battery did reach 36 degrees Celsius, which I'm sure is a result of having many in series and in parallel. The tests were completed using the recommended method. Therefore, I would trust the CHEMID that was matched when you received the report.
Sincerely,
Nick Richards