Other Parts Discussed in Thread: BQ25180
Dear TI experts,
my customer have a question about BQ24032A.
1. Can BQ24032A charge the battery less than 100%, like 80% and terminate charging status?
2. datasheet says that the battery could be recharged if the voltage is under 4.1V, after the charging is complete(4.2V).
Can I change the recharge threshold(4.1V) like 3.9?
Please check this issue. Thanks.
Best regards,
Chase