Part Number: TPS40055
Other Parts Discussed in Thread: LM5146, LM5145,
I have an application in which Voltage Feedforward needs to be disabled due to limitation of maximum duty cycle as a result of programmable UVLO.
I have followed SLUA310 for this purpose with option 2 via section 4.2 to disable voltage feedforard by tieing KFF to BP5 through a resistor Rsub.
What is the effect of tolerance on Rsub ?. i.e. if Rsub is such that Ikff is lower than that calculated by Eq 7 of SLUA310 ? Can you get an unstable situation with irregular PWM ramp ?
Switching frequency of 566kHz. So Rt is 82k as per Eq (1) of the datasheet. Rkff is 27.5k as per Eq (2) of the datasheet and for Vuvlo (Vin(min)) of 8V.
Is Vin in Eq 7 of SLUA310 nominal Vin, or Vin(min). Assuming Vin(min) of 8V, Ikff is 163.3uA. So Rsub is then 9161 ohms according to Eq 8 of SLUA310. We used 9.1k. Unstable PWM operation is observed looking at the SW node.
My main question is what happens if Rsub is greater than 9161 ohms so that Ikff is effectively less than 163.3uA ? Will unstable PWM ramp generation result ? For reliable operation should Rsub be made much less than 9161 ohms ? Should Rsub be recalculated using Vin nominal in Eq 7 of SLUA310 ? Vin nominal is 24V and Vout is 15V for our application. i.e., if Rsub is recalculated for Vin of 24V then Ikff becomes 745uA and Rsub becomes ~2k.
Feedback would be appreciated.
Thanks.