This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R2-DEVICE-FW: TCA fault that will not clear

Part Number: BQ78350-R2-DEVICE-FW

Hi,

I have a few BMS that are throwing TCA and TC faults (TCA and TC are 1).  Looking at the BMS readings, Relative State of Charge is 44%, and Absolute State of Charge is 23%, while FC clear is 95%, and TC clear is also 95%, so we should be under those points.  

Are there other issues that could flag this fault? 

Thanks!